IP.PROTOCOL

This parameter is used to determine the protocol used to connect to the drive.

Examples

Usage

  1. Use Telnet to connect to the drive (default).
  2. Use both SSH and Telnet to connect to the drive.

  • SSH is not fully supported at this time.

Code

Get help on IP.PROTOCOL and then set SSH and Telnet as the allowed protocols to connect to the drive.

--> DRV.HELP IP.PROTOCOL
Help for IP.Protocol [Integer] [NV] [ReadWrite] [Enum] Minval = 0 Maxval = 1 Default = 0 Actual value = 0 (Telnet only) Values = 0 (Telnet only), 1 (Both SSH and Telnet)
--> IP.PROTOCOL 1

Context

For more information on IP configuration for telnet, see Finding and Connecting to a Device.

Versions

Action Version Notes
Implemented 02-03-03-000

 

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also IP.ADDRESS, IP.SUBNET, IP.GATEWAY IP.RESET

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

IP.PROTOCOL

3013h

05h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

IP.PROTOCOL

2204

89C

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

IP.PROTOCOL

2204

Unsigned8

Read/Write

-